Electrical challenges and solutions are often part of residential, industrial and commercial installations. These vary depending on the amount of power involved, the location, the risk it poses to users, and other factors.
Most of the electrical faults pose various risks which range from electric shocks, fires, and loss of property or lives. While the user may avoid using the sections of the installation or equipment that is faulty, it is always advisable to call a qualified electrician to sort out the problem as soon as possible.
Why do electrical problems occur?
Majority of electrical problems result from lack of maintenance, a malpractice, low-quality components, technicians’ faults, or when people choose to ignore the codes and regulations.
Other common electrical challenges may arise due to issues with the electrical generation or the distribution company. These include down lines, poor quality, low or unstable power.
Consumers should have an idea of the common electrical challenges and solutions that transpire during installations. Even when they cannot fix them, they can at least take preventive measures, such as isolating the faulty sections or staying away from the faults.
Typical electrical challenges and solutions
Below are some of the common electrical challenges and solutions at the consumer level. However, it is advisable to always engage qualified electricians to fix the problems and ensure that the wiring is safe and in compliance with all the electrical codes.
Tripping circuit breakers and fuse blowing
When there are faults such as overloading or short circuits, the fuse or breaker keep blowing or tripping. The consumer should ask an experienced electrician to check that the total load does not exceed the breaker or fuse rating, and also confirm that there are no short circuits, broken insulation or faulty equipment.
Loose Connections
The loose connections lead to an unstable flow of power to the appliances. This may occur at the electrical outlet or lighting fixtures, and will lead to continuous equipment reset and flickering of lights. The loose connections can easily damage the electrical appliances and reduce their lifespan. In addition, the arcing between the contacts can lead to fires or electrical burns.
The solution for electrical challenge is to clean the affected conductors and tighten the connection properly.
Incorrect wiring practices
Wrong connections and incorrect sizing of conductors or protection devices can lead to numerous problems. For example, if the fuses and breakers are oversized, they will not provide the protection when they are supposed to. The devices will continue operating as normal even when there is an overload or other overcurrent conditions. The overheating of conductors deteriorates the insulation and has the potential to cause fires.
One way of avoiding this is by hiring qualified electricians who will wire everything according to the codes. However, if you realize that you have wrong connections and incorrect wiring, it is better to look for a different contractor to check the entire installation and rectify the issues.
Crowded electric control panels
As customers add more circuits and load, some electricians have the tendency of overcrowding the panel with extra breakers and wires. This is risky and may lead to overheating of the components inside the panel and eventually malfunctions or even fires.
The solution is to upgrade the panel to a larger size that can accommodate all the circuits.If possible, leave some space for additional circuits in the future.
Using substandard components
The choice of the wiring, outlets, lighting, protection, and others have their contribution to the electrical challenges and solutions. Some electricians use incompatible parts that either does not work or fit properly due to different dimensions, format or rating. The solution is to first identify the improper parts and then replace them with the recommended.
Water, moisture and corrosion
Electricity and water do not mix very well. The presence of moisture around live electrical conductors or parts is always dangerous and people should keep off such areas. If you can safely turn it off, do it to prevent further damage or mishap.
The moisture causes corrosion in the wiring or panel components. This is why it is important to carry out regular safety inspections to identify such areas. The technician should find a way to prevent the moisture or water from getting into the sensitive areas.
Conclusion
There are several common electrical challenges and solutions that technicians should be aware of if they are to provide proper assistance to users. These range from simple connection issues or parts replacements, to more complex problems arising from a number of factors.
While users may not have the end solutions, there are several things they can do to reduce the risks and stay safe until a qualified electrician fixes the problem.