Eaton Recalls 30A and 60A Safety Switches

eaton recalls

Eaton recalls 30A and 60A safety switches that are commonly used for heavy commercial, utility and industrial applications. These were manufactured between November 19, 2018 to January 23, 2018, which were sold in US and Canada.

Affected cataog numbers included in the safety bulletin:

eaton recall
Diagram from Eaton’s Bulletin

According to the bulletin Eaton released, these safety switches can supply power even when the handle is in the “off” position. The error could potentially result in serious injuries or death.

Eaton has clarified that as of July 2, 2018, there were no reports that these safety switches have caused injuries.

The company’s distributors in the US and Canada were notified through an email and advised how to identify whether the safety switch won’t work well.

eaton recall
Diagram from Eaton’s Bulletin
eaton recall
Diagram from Eaton’s Bulletin

All buyers who would like to verify the problem may visit their bulletin or they can contact HdssAdvisoryBulletin@eaton.com, or call Eaton’s Technical Resource Centre at 1-877-ETN-CARE.

This blog is made available for educational purposes ONLY, and is not intended to provide any advice as to product selection, specifications, or appropriate uses. We assume no liability for any loss or damage resulting from one’s reliance on the material provided. Please note that such material is not updated regularly and that some of the information may not be current. We do not control or endorse and are not responsible for third-party websites linked herein.

Be the first to comment

Leave a Reply

Your email address will not be published.


*